Description
This Tcl command copies a device in the chain to the clipboard. Chain programming mode must be set. See the paste_device command for more information.
copy_device -name {name}
Arguments
Parameter | Type | Description |
---|
name | string | Specifies the device name. You can repeat this argument to copy multiple devices. This paramater is mandatory. |
Return Type | Description |
---|
None | None |
Error Codes
Error Code | Description |
---|
None | Required parameter 'name' is missing. |
None | The device with name 'test_name' doesn't exist. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'copy_device [-name "name"]+'. |
Supported Families
Supported Families |
PolarFire® |
PolarFire SoC |
RTG4™ |
SmartFusion® 2 |
IGLOO® 2 |
Example
The example copies the device 'MyDevice1' to the same location with a new name 'MyDevice2'.
copy_device -name {MyDevice1} -name {MyDevice2}