Description
This Tcl command automatically starts chain construction for the specified programmer.
construct_chain_automatically -name {name}
Arguments
Parameter | Type | Description |
---|
name | string | Specifies the programmer(s) name(s). You can repeat this argument to specify multiple programmers names. |
Return Type | Description |
---|
None | None |
Error Codes
Error Code | Description |
---|
None | Required parameter 'name' is missing. |
None | Parameter 'name' is missing or has invalid value. |
None | Parameter 'name' has illegal value. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'construct_chain_automatically [-name "name"]+'. |
Supported Families
Supported Families |
PolarFire® |
PolarFire SoC |
RTG4™ |
SmartFusion® 2 |
IGLOO® 2 |
Example
For a single programmer:
construct_chain_automatically -name {E2004NSXB1}
See Also
- scan_chain_prg
- enable_device
- set_debug_programmer
- set_device_name
- set_programming_file
- set_programming_action
- run_selected_actions