3.5.1.14 Memory Partitioning
(Ask a Question)Memory Partitioning is an optimization where aggregate types such as arrays and structs are partitioned into smaller pieces allowing for a greater number of reads and writes (accesses) per cycle. SmartHLS™ instantiates a RAM for each aggregate type where each RAM has up to two ports (allowing up to two reads/writes per cycle). Partitioning aggregate types into smaller memories or into its individual elements allows for more accesses per cycle and improves memory bandwidth.
Important: There are two flavors of memory partitioning, access-based partitioning and user-specified partitioning.
- Accessing memory outside of an array dimension is not supported by memory partitioning and will sometimes cause incorrect circuit behavior. An example of this is casting a 2-d array to a pointer and iterating through the size of the 2-d array.
- Pointers that alias to different memories (e.g. a function called with different memories) or different sections of the same memory (for example, a pointer that is assigned to multiple memories based on a condition) can be partitioned if the aliased memories/sections have the same partitions. Otherwise, access-based partitioning will not partition the aliased memories, or a warning will be displayed for user-specified partitioning. The following example shows an unsupported aliasing case:
int sum_array(int *z) { #pragma HLS function noinline int sum = 0; for (int i = 0; i < 100; i++) sum += z[i]; return sum; } int main() { #pragma HLS function top #pragma HLS memory partition variable(x) type(block) dim(1) factor(2) int x[100]; // x should be partitioned into 2 partitions #pragma HLS memory partition variable(x) type(cyclic) dim(1) factor(4) int y[100]; // x should be partitioned into 4 partitions // ... int sum_x = sum_array(x); int sum_y = sum_array(y); // ... }
SmartHLS will output a warning:
Warning: The user specified memory "x" on line 80 of test.cpp could not be partitioned because the memory aliases with another memory at line 71 of test.cpp that has a different partitioning. Warning: The user specified memory "y" on line 82 of test.cpp could not be partitioned because the memory aliases with another memory at line 71 of test.cpp that has a different partitioning.
- Partitions with no accesses are discarded.