3.5.1.10 Data Flow Parallelism
(Ask a Question)Data Flow or "dataflow" parallelism is another commonly used technique to improve hardware throughout. In dataflow parallelism, a succession of computational tasks which process continuous streams of data can execute in parallel. These tasks are called dataflow sub-functions. A function is declared as a dataflow function using the pragma #pragma HLS function dataflow
(see 3.6.1.11 Dataflow ). Within this dataflow function, the called functions, or sub-functions, will execute with dataflow parallelism. If the dataflow function contains loops or control-flow, each top-level loop nest or control-flow region will be extracted into a new sub-function.
In a dataflow circuit, synchronization will be required for passing intermediate data between the sub-functions that can run in parallel. For instance, a producer sub-function can write to an array for another consumer sub-function to read. In this case, the consumer sub-function needs to "know" that the producer has finished writing the array in order to start. SmartHLS™ can convert such intermediate data into double/shared buffer or FIFOs. By default, intermediate data is converted into double buffer. see 3.6.1.12 Dataflow Channel pragma.
- The dataflow function and all its sub-functions must have
void
return type, with output data passed by pointer or by reference. - Nested dataflow functions must have the parent dataflow function directly calling the child dataflow function. That is, it is supported for a dataflow function to call another dataflow function; however it is not allowed to have a dataflow function, calling a non-dataflow function, which further calls a dataflow function.
- Sub-functions cannot contain SmartHLS Threads (to use SmartHLS Threads, see 3.5.1.11 Multi-threading with SmartHLS Threads).
When a dataflow function is called from within a loop, the loop body can only contain that call in order for SmartHLS to overlap the invocations of the dataflow function; otherwise the dataflow function will still run in a non-overlapped manner.
- Data external to the dataflow function (declared outside of the dataflow function and its sub-functions) can only be accessed by 1 sub-function, unless the data is of FIFO type.
- All intermediate data should have exactly one producer and one consumer sub-function.
- When configuring an intermediate data variable, that is, an array or single-element memory to be implemented as a FIFO channel using the 3.6.1.12 Dataflow Channel pragma, it is only correct to use the
fifo
type when:- The producer function only writes to the variable in a sequential manner.
- The consumer function only reads from the variable in a sequential manner.
- If a sub-function calls another synthesizable sub-sub-function, the sub-sub-function will be automatically inlined by SmartHLS.
- If a sub-function is called in more than one location inside a dataflow function, the sub-function will be automatically replicated by SmartHLS.
Dataflow parallelism can be used to overlap sub-functions which run in sequence, or to run independent sub-functions in parallel.