argument | string | No | - | Argument name |
type | axi_target | No | - | Interface type |
num_elements | integer | Yes | - | Specifies the number of elements of the argument array. Can override the array size in the argument. Only needed by the 3.5.1.7 Simulate HLS Hardware (SW/HW Co-Simulation) feature and does not affect HLS-generated RTL. |
ptr_addr_interface | simple|axi_target | Yes | - | Specifies the interface type for setting the base address of the accessing memory. The default type is simple but is changed to axi_target if 3.6.1.19 Default All Interfaces to Use AXI4 Target is set. |
max_burst_len | integer | Yes | 16 | Specifies the maximum burst length for each AXI initiator transaction. Transfers that are larger than the maximum burst length will be split into multiple AXI transactions. The permitted values are between 1 and 256. |
max_outstanding_reads | integer | Yes | 1 | Specifies the maximum amount of read burst requests to external AXI4 Targets that can be left outstanding (waiting for response) before the accelerator stalls. This infers a FIFO of size max_outstanding_reads*addr_size for the AR channel, and a FIFO of size max_outstanding_reads*max_burst_len*word_size for the R channel. The permitted values are between 1 and 8. |
max_outstanding_writes | integer | Yes | 1 | Specifies the maximum amount of write burst requests to external AXI4 Targets that can be left outstanding (waiting for response) before the accelerator stalls. This infers a FIFO of size max_outstanding_writes*addr_size for the AW channel, and a FIFO of size max_outstanding_writes*max_burst_len*word_size for the W channel. The permitted values are between 1 and 8. |
add_4k_boundary_protection | bool | Yes | true | Specifies whether or not SmartHLS™ should generate additional logic to protect AXI4 initiator burst transactions from crossing 4K boundaries for this argument. Setting this field to false will remove this alignment logic, but the user must then make sure that any pointer addresses given to the SmartHLS module will not result in bursting accross a 4K address boundary (a violation of the AXI4 spec. |