9.9.1.1.2 Highlighting

The Highlighting option allows you to set persistent colors on designated macros, nets, or both across the system.

To set a highlight, go to the Logical Object Browser or the Net Object Browser, select one or more macros and/or components, and click the pencil icon as shown in the following toolbar.
Figure 9-32. Pencil and Eraser Icons

When you set a highlight, all selected macros, ports, and/or nets in the design are marked with the selected color. The selected color appears in the left object browser tree. The following figure shows the left Main Object Browser with the logical tree displayed. To select both components, click one component, hold down the Ctrl key and click the other component.

Figure 9-33. Example of Highlighting Shown in the Object Browser Tree
The color remains until you select one of the two middle eraser icons:
  • The left eraser icon removes all highlights.
  • The right eraser icon removes highlights only from selected items.

To set the highlights, use the Current Highlight check box from the Design Settings docking window. Below this check box are an Auto Rotate check box, along with eight Highlight check boxes and radio buttons.
  • Use the Highlight check boxes to enable or disable a highlight. Separate check boxes are provided for macros and nets.
  • Use the Highlight radio buttons to designate which highlight is active.
Note: You cannot disable the active highlight.
Figure 9-34. Design Settings Docking Window

Clicking the colored box next to each check box allows you to select a color for that macro or net.

The following figure shows an example of the results when all options under Nets are exposed.
Figure 9-35. Example of Exposing All Nets
If Net Settings is not checked, all nets in the system, except cross-probe nets, are disabled. All options subordinate to that option are marked with a gray box to show that the option is not used. If Show Nets for Highlighted Macros is not checked, all net options inside the currently highlighted net selections are disabled. To restore the color of these options, check the individual options. If you check Show Nets for Highlighted Macros, the individual settings in the highlight settings area determine whether nets will be drawn.
Note: If you enable Auto Rotate and Net under Auto Rotate, and then uncheck the check box in the Net color selection, the net color in the Net view is not consistent with that of the Planner.
The Consolidate Globals option converts the raw clock display with globals connected to locals as if the sum of the local nets and the global nets are the same net. This is for display purposes only.
The bottom three options in the Design Settings docking window work with groups of macros and ports for which you consider net lines as a single entity:
  • Show Interior Nets for Selected/Highlighted Macros shows lines that connect two different macros in the group.
  • Show Input Nets for Selected/Highlighted Macros shows lines that connect an output port of an exterior macro to one or more input pins in the group.
  • Show Driver Nets for Selected/Highlighted Macros shows drivers in the group that connect with an exterior macro.