21.4.5 sd_configure_core_instance
(Ask a Question)Description
This tcl command configures the parameters of a core instance (Direct Instantiation) in a SmartDesign component. This command can configure multiple core parameters at a time.
sd_configure_core_instance -sd_name {smartdesign component name} \
-instance_name {core instance name} \
-params {core parameters}
Arguments
Parameter | Type | Description |
---|---|---|
sd_name | string | Specifies the name of the SmartDesign component. It is mandatory. |
instance_name | string | Specifies the name of the core instance in the SmartDesign which needs to be configured. It is mandatory. |
params | string | Specifies the parameters that need to be configured for the core instance. It is mandatory. |
Return Type | Description |
---|---|
None | None |
Error Codes
Error Code | Description |
---|---|
None | Required parameter 'sd_name' is missing. |
None | Parameter 'sd_name' has illegal value. |
None | Required parameter 'instance_name' is missing. |
None | Parameter 'instance_name' has illegal value. |
None | The component 'comonent_name' doesn't exist. |
None | Parameter 'params' has illegal value. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'sd_configure_core_instance -sd_name "sd_name" -instance_name "instance_name" [-params "[params]+"] . |
Supported Families
Supported Families |
---|
PolarFire® |
PolarFire SoC |
RTG4™ |
SmartFusion® 2 |
IGLOO® 2 |
Example
This example configures {COREFIFO_0} instance in the {SD1} SmartDesign component with the following parameters: "SYNC:0", "param2:value2" and "param3:value3".
sd_configure_core_instance \
-sd_name {SD1} \
-instance_name {COREFIFO_0} \
-params {"SYNC:0" "param2:value2" "param3:value3"}