21.4.54 sd_show_bif_pins
(Ask a Question)Description
This tcl command exposes one or more internal scalar or bus pins/ports of a Bus Interface pin/port. A Bus Interfacepin/port is usually a group of normal scalar or bus pins/ports grouped together and used to connect instances thathave similar interfaces.
This command will not expose multiple pins/ports in release v2021.1. Support to expose multiple scalar or bus pins/portswill be provided in the next Libero release.
sd_show_bif_pins -sd_name {smartdesign component name} \
-bif_pin_name {name of the bif pin or port} \
-pin_names {pins or ports to be exposed}
Arguments
Parameter | Type | Description |
---|---|---|
sd_name | string | Specifies the name of the SmartDesign component. It is mandatory. |
bif_pin_name | string | Specifies the name of the Bus Interface pin/port for which the internal pins/ports need to be exposed. It is mandatory. |
pin_names | string | Specifies the names of the Bus Interface internal pins/ports to be exposed. It is mandatory. |
Return Type | Description |
---|---|
None | None |
Error Codes
Error Code | Description |
---|---|
None | Parameter 'pin_names' has illegal value. |
None | Required parameter 'pin_names' is missing. |
None | Parameter 'bif_pin_name' has illegal value. |
None | Required parameter 'bif_pin_name' is missing. |
None | Parameter 'sd_name' has illegal value. |
None | Required parameter 'sd_name' is missing. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'sd_show_bif_pins -sd_name "sd_name" -bif_pin_name "bif_pin_name" -pin_names "pin_names"'. |
Supported Families
Supported Families |
---|
PolarFire® |
PolarFire SoC |
RTG4™ |
SmartFusion® 2 |
IGLOO® 2 |
Example
This example exposes "COREAXI4INTERCONNECT_C0_0:MASTER0_AWADDR" pin for "COREAXI4INTERCONNECT_C0_0:AXI4mmaster0" bif pin.
sd_show_bif_pins -sd_name {top} \
-bif_pin_name {COREAXI4INTERCONNECT_C0_0:AXI4mmaster0} \
-pin_names {COREAXI4INTERCONNECT_C0_0:MASTER0_AWADDR}
See Also
sd_delete_bif_pin