21.4.53 sd_save_core_instance_config
(Ask a Question)Description
This Tcl command is used to save the core instance configuration specified using one or more 'sd_configure_core_instance' commands. This command is typically used after configuring a core instance in a SmartDesign, to save that core instance's configuration.
sd_save_core_instance_config -sd_name {smartdesign component name} \
-instance_name {core instance name}
Arguments
Parameter | Type | Description |
---|---|---|
sd_name | string | Specifies the name of the SmartDesign component. It is mandatory. |
instance_name | string | Specifies the name of the core instance in the SmartDesign for which the configuration must be saved. It ismandatory. |
Return Type | Description |
---|---|
None | None |
Error Codes
Error Code | Description |
---|---|
None | Parameter 'instance_name' has illegal value. |
None | Required parameter 'instance_name' is missing. |
None | Parameter 'sd_name' has illegal value. |
None | Required parameter 'sd_name' is missing. |
None | Parameter 'param_name' is not defined. Valid command formatting is'sd_save_core_instance_config -sd_name "sd_name" -instance_name "instance_name"'. |
Supported Families
Supported Families |
---|
PolarFire® |
PolarFire SoC |
RTG4™ |
SmartFusion® 2 |
IGLOO® 2 |
Example
This example saves "COREFIFO_0" core instance configuration.
sd_save_core_instance_config -sd_name {SD1} -instance_name {COREFIFO_0}