Description
This tcl command removes one or more pins from a pin group on an instance in a SmartDesign component.
sd_remove_pins_from_group -sd_name {smartdesign component name} \
-instance_name {instance name} \
-group_name {group name} \
-pin_names {pin names}
Arguments
Parameter | Type | Description |
---|
sd_name | string | Specifies the name of the SmartDesign component. It is mandatory. |
instance_name | string | Specifies the name of the instance on which the pin group is present. It is mandatory. |
group_name | string | Specifies the name of the pin group from which pins need to be removed. It is mandatory. |
pin_names | string | Specifies the list of pin names to be removed from the pin group(example below). It is mandatory. |
Return Type | Description |
---|
None | None |
Error Codes
Error Code | Description |
---|
None | Parameter 'param_name' is not defined. Valid command formatting is 'sd_remove_pins_from_group -sd_name "sd_name" -instance_name "instance_name" [-group_name "group_name"] [-pin_names "[pin_names]+"]'. |
None | Required parameter 'sd_name' is missing. |
None | Required parameter 'instance_name' is missing. |
None | The component 'component_name' doesn't exist. |
SDCTRL05 | Pin 'group_name' does not exist. |
Supported Families
Supported Families |
---|
PolarFire® |
PolarFire SoC |
RTG4™ |
SmartFusion® 2 |
IGLOO® 2 |
Example
The following example removes "ARESETN ACLK" pin from "MyGroup", that is on "COREAXINTERCONNECT_C0_0" instance, in the "TOP" design:
sd_remove_pins_from_group -sd_name {TOP} \
-instance_name {COREAXINTERCONNECT_C0_0} \
-group_name {Group} \
-pin_names {ARESETN ACLK}
The following example removes "WA_RSTn", "DISP_SEL" pins from "MyGroup", that is on "CorePCS_C0_0" instance, in the "TOP" design:
sd_remove_pins_from_group -sd_name {TOP} \
-instance_name {CorePCS_C0_0} \
-group_name {MyGroup} \
-pin_names {"WA_RSTn" "DISP_SEL"}
See Also
- sd_create_pin_group
- sd_add_pins_to_group