21.4.22 sd_delete_instances
(Ask a Question)Description
This tcl command deletes one or more instances from a SmartDesign component.
Note: This command is not required to build a
SmartDesign component. This command maps to an interactive user action in the
SmartDesign Canvas and will not be present in the exported SmartDesign component Tcl
description.
sd_delete_instances -sd_name {smartdesign component name} \
-instance_names {instance names}
Arguments
Parameter | Type | Description |
---|---|---|
sd_name | string | Specifies the name of the SmartDesign component. It is mandatory. |
instance_names | string | Specifies the instance names to be deleted. It is mandatory. |
Return Type | Description |
---|---|
None | None |
Error Codes
Error Code | Description |
---|---|
None | Parameter 'instance_names' has illegal value. |
None | Required parameter 'instance_names' is missing. |
None | Parameter 'sd_name' has illegal value. |
None | Required parameter 'sd_name' is missing. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'sd_delete_instances -sd_name "sd_name" -instance_names "[instance_names]+"'. |
Supported Families
Supported Families |
---|
PolarFire® |
PolarFire SoC |
RTG4™ |
SmartFusion® 2 |
IGLOO® 2 |
Example
This example deletes "RAM64X12_0" instance.
sd_delete_instances -sd_name {top} \
-instance_names {RAM64X12_0}
See Also
- sd_disconnect_instance
- sd_duplicate_instance