Description
This Tcl command sets synthesis attribute to the specified port of the specified SmartDesign. The attribute is added in the HDL file at the component generation.
sd_set_port_synth_attr \
-sd_name {SmartDesign component name} \
-port_name {port name} \
-attr_name {synthesis attribute name} \
-attr_value {synthesis attribute value}
Arguments
Parameter | Type | Description |
---|
sd_name | string | This argument is used to specify the name of the SmartDesign component in which the port synthesis attribute is set. This is a mandatory argument. |
port_name | string | Name of the port in SmartDesign that synthesis attribute is added to. This is a mandatory argument. |
attr_name | string | Synthesis attribute to be added. This is a mandatory argument. |
attr_value | string | Value of the attribute. Some attributes do not require values. This is a mandatory argument. |
Synthesis Attributes
The following is the list of attributes and directives available in the Synopsys® FPGA synthesis tool that are supported by SmartDesign.
Name |
Object |
Attribute/Directive |
syn_insert_buffer |
port, instance |
Attribute |
syn_keep |
net |
Directive |
syn_maxfan |
port, net, instance, register |
Attribute |
syn_no_compile_point |
module/architecture |
Attribute |
syn_noclockbuf |
port, net, module/architecture |
Attribute |
syn_noprune |
instance, module/architecture |
Directive |
syn_preserve |
register, port, module/architecture |
Directive |
Return Type | Description |
---|
None | None |
Error Codes
Error Code | Description |
---|
SDCTRL05 | Pin 'port_name' does not exist. |
None | Parameter 'port_name' has illegal value. |
None | Required parameter 'port_name' is missing. |
None | Parameter 'attr_value' has illegal value. |
None | Required parameter 'attr_value' is missing. |
None | Parameter 'attr_name' has illegal value. |
None | Required parameter 'attr_name' is missing. |
None | Parameter 'sd_name' has illegal value. |
None | Required parameter 'sd_name' is missing. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'sd_set_port_synth_attr -sd_name "sd_name" -attr_name "attr_name" -attr_value "attr_value" -port_name "port_name"'. |
Supported Families
Supported Families |
---|
PolarFire® |
PolarFire SoC |
RTG4™ |
SmartFusion® 2 |
IGLOO® 2 |
Example
This example sets "syn_keep" attribute with "false" value on the "PRESETN" port in the "top" design.
sd_set_port_synth_attr -sd_name {top} -attr_name {syn_keep} \
-attr_value {false} -port_name {PRESETN}
See Also
- sd_remove_port_synth_attr