21.6.3 CONFIGURE_PROG_OPTIONS
(Ask a Question)Description
"CONFIGURE_PROG_OPTIONS" is a command tool used in configure_tool. It sets the programming options for PolarFire, PolarFire SoC, RTG4, SmartFusion 2 and IGLOO 2 devices.
The command usage for the PolarFire is the following:
configure_tool -name {CONFIGURE_PROG_OPTIONS} \
-params {design_version:<value>} \
-params {back_level_version:<value>} \
-params {silicon_signature:<value>}The command usage for the SmartFusion 2 and IGLOO 2 is the following:
configure_tool -name {CONFIGURE_PROG_OPTIONS} \
-params {design_version:<value>} \
-params {enable_auto_update:true | false} \
-params {enable_prog_recovery:true | false} \
-params {silicon_signature:<value>} \
-params {spi_clk_freq:<value>} \
-params {spi_data_transfer_mode:<value>}The command usage for the RTG4 is the following:
configure_tool -name {CONFIGURE_PROG_OPTIONS} \
-params {design_version:<value>} \
-params {disable_digest_check:<value>} \
-params {disable_fabric_erase_write_verify:<value>} \
-params {disable_jtag:<value>} \
-params {disable_probe_read_write:<value>} \
-params {disable_spi:<value>} \
-params {one_time_programmable:<value>} \
-params {silicon_signature:<value>} \
-params {system_controller_suspend_mode:<value>}Arguments
The following table list the "CONFIGURE_PROG_OPTIONS" arguments for PolarFire.
| Parameter | Type | Description | 
|---|---|---|
| design_version | Integer {0 through 65535} | Sets the design version. It must be greater than the Back Level version in SPM Update Policy. | 
| back_level_version | Integer {0 through 65535} | Sets the back level version. | 
| silicon_signature | Hex {<max length 8 Hex characters>} | 32-bit (8 hex characters) silicon signature to be programmed into the device. This field can be read from the device using the JTAG USERCODE instruction. | 
The following table list the "CONFIGURE_PROG_OPTIONS" arguments for SmartFusion 2/IGLOO 2.
| Parameter | Type | Description | 
|---|---|---|
| design_version | Integer {0 through 65535} | Sets the design version. It must be greater than the Back Level version in SPM Update Policy. | 
| silicon_signature | Hex {<max length 8 Hex characters>} | 32-bit (8 hex characters) silicon signature to be programmed into the device. This field can be read from the device using the JTAG USERCODE instruction. | 
| enable_auto_update | boolean | Sepcify "TRUE" or 1 to enable auto update, spceify "FALSE" or 0 to disable auto update. This parameter is available for SmartFusion 2. | 
| enable_prog_recovery | boolean | Sepcify "TRUE" or 1 to enable programming recovery, spceify "FALSE" or 0 to disable programming recovery. This parameter is available for SmartFusion 2. | 
| spi_clk_freq | double | Sets SPI clock frequency from a list of possible values {1.00 | 2.08 | 3.13 | 4.16 | 5.00 | 6.25 | 8.30 | 12.50 | 25.00 }. This parameter is available for SmartFusion 2. | 
| spi_data_transfer_mode | binary | SPI data transfer mode sets the values for SPS, SPO and SPH in the UI. SPS has a fixed value of 1 and cannot be changed. The user can change the value of only SPO and SPH to 0 or 1. The acceptable value are the following: {100 | 101 | 111 | 110}. This parameter is available for SmartFusion 2. | 
The following table list the "CONFIGURE_PROG_OPTIONS" arguments for RTG4.
| Parameter | Type | Description | 
|---|---|---|
| design_version | Integer {0 through 65535} | Sets the design version. It must be greater than the Back Level version in SPM Update Policy. | 
| silicon_signature | Hex {<max length 8 Hex characters>} | 32-bit (8 hex characters) silicon signature to be programmed into the device. This field can be read from the device using the JTAG USERCODE instruction. | 
| disable_digest_check | boolean | Enable or disable digest check. | 
| disable_fabric_erase_write_verify | boolean | Enable or disable Fabric Erase/Write/Verify. | 
| disable_jtag | boolean | Enable or disable JTAG interface. | 
| disable_probe_read_write | boolean | Enable or disable Probe Read/Write. | 
| disable_spi | boolean | Enable or disable SPI interface. | 
| one_time_programmable | boolean | Set "true" or 1 to make the device one-time programmable.  Note: After programming the device you will NOT be able to erase or program the device. You will be able to run programming actions VERIFY and VERIFY_DIGEST as well as use SmartDebug to debug with probes and read the digest of the Fabric.  | 
| system_controller_suspend_mode | boolean | Enable or disable System Controller Suspend mode. | 
| Return Type | Description | 
|---|---|
| Integer | Returns 0 on success and 1 on failure. | 
Error Codes
| Error Code | Description | 
|---|---|
| None | Incorrect Back Level version value format. | 
| None | Back Level version must be less than or equal to Design version. | 
| None | parameter disable_spi does not exist (PolarFire). | 
| None | parameter one_time_programmable does not exist (PolarFire). | 
| None | Incorrect Design version value format. | 
| None | Design version value must be between 0 and 65535. | 
| None | Silicon signature must be max 8 HEX chars. | 
| None | Illegal SPI clock frequency '1.11 MHz'. | 
| None | Programming Recovery must be enabled to allow Auto Update. | 
| None | Silicon signature must be max 8 HEX chars. | 
| None | Unknown SPI data transfer mode: SPS(0) SPO(0) SPH(0). | 
Supported Families
| Supported Families | 
|---|
| PolarFire® | 
| PolarFire SoC | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
Example
The following example configures programming parameters for the PolarFire device:
configure_tool -name {CONFIGURE_PROG_OPTIONS} \
               -params {design_version:255} \
               -params {back_level_version:200} \
               -params {silicon_signature:abcdef}The following example configures programming parameters for the SmartFusion 2 device:
configure_tool -name {CONFIGURE_PROG_OPTIONS}\
               -params {design_version:255}
               -params {enable_auto_update:true}
               -params {enable_prog_recovery:true}
               -params {silicon_signature:abcdef}
               -params {spi_clk_freq:25.00}
               -params {spi_data_transfer_mode:100}See Also
- CONFIGURE_ACTIONS_PROCEDURES
 - set_programming_action