Description
"EXPORTNETLIST" is a command tool used in the run_tool command. This command exports a
                    *.v or *.vhd netlist file to the active
                synthesis implementation folder.
run_tool -name {EXPORTNETLIST}
Arguments
| Parameter | Type | Description | 
|---|
| None | None | None | 
| Return Type | Description | 
|---|
| Integer | Returns 0 on success and 1 on failure. | 
Error Codes
| Error Code | Description | 
|---|
| None | None | 
Supported Families
            
            | Supported Families | 
|---|
| PolarFire® | 
| PolarFire SoC | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
 
        Example
The following command exports netlist file:
run_tool -name {EXPORTNETLIST}