21.6.25 VERIFYTIMING
(Ask a Question)Description
"VERIFYTIMING" is a command tool used in configure_tool and run_tool. Use "configure_tool -name {VERIFYTIMING}" to configure "VERIFYTIMING" tool, run_tool passes a script file that contains timing specific Tcl commands to the VERIFYTIMING command and executes it.
-params argument for multiple parameters.configure_tool -name {VERIFYTIMING} -params {parameter:value}
run_tool -name {VERIFYTIMING} -script {timing.tcl}Where, timing.tcl is a script that contains the SmartTime-specific Tcl commands. You can include SmartTime-specific Tcl commands to create user path, to set and generate timing reports.
Arguments
The following table list the "VERIFYTIMING" arguments for PolarFire, SmartFusion 2, IGLOO 2, RTG4 and PolarFire SoC.
| Parameter | Type | Description | 
|---|---|---|
| MAX_TIMING_MULTI_CORNER | boolean | Max Delay Static Timing Analysis report based on multi-corners. Specify 0 or "False" to turn report generation OFF and 1 or "True" to turn it ON. Default is 1. | 
| MAX_TIMING_VIOLATIONS_MULTI_CORNER | boolean | Max Delay Static Timing Analysis violation report based on multi-corners. Specify 0 or "False" to turn report generation OFF and 1 or "True" to turn it ON. Default is 1. | 
| MIN_TIMING_MULTI_CORNER | boolean | Min Delay Static Timing Analysis report based on multi-corners. Specify 0 or "False" to turn report generation OFF and 1 or "True" to turn it ON. Default is 1. | 
| MIN_TIMING_VIOLATIONS_MULTI_CORNER | boolean | Min Delay Static Timing Analysis violation report based on multi-corners. Specify 0 or "False" to turn report generation OFF and 1 or "True" to turn it ON. Default is 1. | 
| MAX_TIMING_SLOW_LV_HT | boolean | Max Delay Static Timing Analysis report based on Slow process, Low Voltage, and High Temperature operating conditions. Specify 0 or "False" to turn report generation OFF and 1 or "True" to turn it ON. Default is 1. | 
| MIN_TIMING_FAST_HV_LT | boolean | Min Delay Static Timing Analysis report based on Fast process, High Voltage, and Low Temperature operating conditions. | 
| MAX_TIMING_FAST_HV_LT | boolean | Max Delay Static Timing Analysis report based on Fast process, High Voltage, and Low Temperature operating conditions. Specify 0 or "False" to turn report generation OFF and 1 or "True" to turn it ON. Default is 0. | 
| MIN_TIMING_SLOW_LV_HT | boolean | Min Delay Static Timing Analysis report based on Slow process, Low Voltage and High Temperature operating conditions. Specify 0 or "False" to turn report generation OFF and 1 or "True" to turn it ON. Default is 0. | 
| MAX_TIMING_VIOLATIONS_SLOW_LV_HT | boolean | Max Delay Static Timing Analysis violation report based on Slow process, Low Voltage and High Temperature operating conditions. Specify 0 or "False" to turn report generation OFF and 1 or "True" to turn it ON. Default is 0. | 
| MIN_TIMING_VIOLATIONS_FAST_HV_LT | boolean | Min Delay Static Timing Analysis violation report based on Fast process, High Voltage and Low Temperature operating conditions. Specify 0 or "False" to turn report generation OFF and 1 or "True" to turn it ON. Default is 0. | 
| MAX_TIMING_VIOLATIONS_FAST_HV_LT | boolean | Max Delay Static Timing Analysis violation report based on Fast process, High Voltage and Low Temperature operating conditions. Specify 0 or "False" to turn report generation OFF and 1 or "True" to turn it ON. Default is 0. | 
| MIN_TIMING_VIOLATIONS_SLOW_LV_HT | boolean | Min Delay Static Timing Analysis violation report based on Slow process, Low Voltage and High Temperature operating conditions. Specify 0 or "False" to turn report generation OFF and 1 or "True" to turn it ON. Default is 0. | 
| MAX_EXPANDED_PATHS_TIMING | integer | Sets the number of expanded paths under each section. The number of paths set can be anywhere from 1 to 20000. Default is 5. | 
| MAX_EXPANDED_PATHS_VIOLATION | integer | Sets the number of expanded paths under each section. The number of paths set can be anywhere from 0-20000. Default is 20. | 
| MAX_PARALLEL_PATHS_TIMING | integer | Sets the number of parallel paths for each expanded path. | 
| MAX_PARALLEL_PATHS_VIOLATION | integer | Sets the number of parallel paths for each expanded path. The number of paths set can be anywhere from 1-20000. Default is 1. | 
| MAX_PATHS_TIMING | integer | Sets the number of reported paths under each section. The number of paths set can be anywhere from 1- 20000. Default is 10. | 
| MAX_PATHS_VIOLATION | integer | Sets the number of reported paths under each section. The number of paths set can be anywhere from 1- 20000. Default is 20. | 
| SLACK_THRESHOLD_VIOLATION | real | Sets a maximum slack threshold value in nanoseconds. Paths will be filtered based on the slack threshold value only in Timing Violation reports. Value entered is a real number. | 
| CONSTRAINTS_COVERAGE | boolean | Constraint Timing Coverage report. | 
| FORMAT | string | Selects the format for the Timing Report: Text(txt), XML(xml), CSV(csv) or HTML(html) format. | 
| SMART_INTERACTIVE | boolean | When SMART_INTERACTIVE parameter is set to 1. The verify timing tool opens timing report explorer interactively and reports timing paths. Available from Libero v12.6+. | 
| MAX_PATHS_INTERACTIVE_REPORT | integer | Specifies maximum number of path in the max and min analysis. The default value is set to 1000. The Range is 1-10000. Available from Libero v12.6+. | 
The following table list the "VERIFYTIMING" arguments for PolarFire and PolarFire SoC.
| Parameter | Type | Description | 
|---|---|---|
| MAX_TIMING_SLOW_LV_LT | boolean | Max Delay Static Timing Analysis report based on Slow process, Low Voltage, and Low Temperature operating conditions. Specify 0 or "False" to turn report generation OFF and 1 or "True" to turn it ON. Default is 1. | 
| MIN_TIMING_SLOW_LV_LT | boolean | Min Delay Static Timing Analysis report based on Slow process, Low Voltage and Low Temperature operating conditions. Specify 0 or "False" to turn report generation OFF and 1 or "True" to turn it ON. Default is 0. | 
| MAX_TIMING_VIOLATIONS_SLOW_LV_LT | boolean | Max Delay Static Timing Analysis violation report based on Slow process, Low Voltage and Low Temperature operating conditions. Specify 0 or "False" to turn report generation OFF and 1 or "True" to turn it ON. Default is 0. | 
| MIN_TIMING_VIOLATIONS_SLOW_LV_LT | boolean | Min Delay Static Timing Analysis violation report based on Slow process, Low Voltage and Low Temperature operating conditions. Specify 0 or "False" to turn report generation OFF and 1 or "True" to turn it ON. Default is 0. | 
| Return Type | Description | 
|---|---|
| Integer | "configure_tool -name {VERIFYTIMING}" returns 0 on success and 1 on failure. "run_tool -name {VERIFYTIMING} -script {<timing.tcl>}" returns 0 on success and 1 on failure. | 
Error Codes
| Error Code | Description | 
|---|---|
| None | Required parameter 'params' is missing. | 
| None | FORMAT is set to an illegal value 'forma_value'. Formats for timing reports generation are XML, TEXT, HTML and CSV. | 
| None | MAX_EXPANDED_PATHS_TIMING is set to an illegal value 'value'. Legal values must be between 1 and 200000. | 
| None | MAX_PARALLEL_PATHS_VIOLATION is set to an illegal value 'values'. Legal values must be between 1 and 200000. | 
| None | MAX_PARALLEL_PATHS_TIMING is set to an illegal value 'value'. Legal values must be between 1 and 200000. | 
| None | MAX_PATHS_VIOLATION is set to an illegal value 'value'. Legal values must be between 1 and 200000. | 
| None | MAX_PATHS_TIMING is set to an illegal value 'value'. Legal values must be between 1 and 200000. | 
| None | MAX_TIMING_FAST_HV_LT is set to an illegal value 'value'. Legal value are true, false, 0 or 1. | 
| None | MAX_TIMING_MULTI_CORNER is set to an illegal value 'value'. Legal value are true, false, 0 or 1. | 
| None | MAX_TIMING_SLOW_LV_HT is set to an illegal value 'value'. Legal value are true, false, 0 or 1. | 
| None | MAX_TIMING_SLOW_LV_LT is set to an illegal value 'value'. Legal value are true, false, 0 or 1. | 
| None | MAX_TIMING_VIOLATIONS_SLOW_LV_LT is set to an illegal value 'value'. Legal value are true, false, 0 or 1. | 
| None | MAX_TIMING_VIOLATIONS_SLOW_LV_HT is set to an illegal value 'value'. Legal value are true, false, 0 or 1. | 
| None | MAX_TIMING_VIOLATIONS_MULTI_CORNER is set to an illegal value 'value'. Legal value are true, false, 0 or 1. | 
| None | MAX_TIMING_VIOLATIONS_FAST_HV_LT is set to an illegal value 'value'. Legal value are true, false, 0 or 1. | 
| None | MIN_TIMING_SLOW_LV_LT is set to an illegal value 'value'. Legal value are true, false, 0 or 1. | 
| None | MIN_TIMING_SLOW_LV_HT is set to an illegal value 'value'. Legal value are true, false, 0 or 1. | 
| None | MIN_TIMING_MULTI_CORNER is set to an illegal value 'value'. Legal value are true, false, 0 or 1. | 
| None | MIN_TIMING_FAST_HV_LT is set to an illegal value 'value'. Legal value are true, false, 0 or 1. | 
| None | MIN_TIMING_VIOLATIONS_SLOW_LV_LT is set to an illegal value 'value'. Legal value are true, false, 0 or 1. | 
| None | MIN_TIMING_VIOLATIONS_SLOW_LV_HT is set to an illegal value 'value'. Legal value are true, false, 0 or 1. | 
| None | MIN_TIMING_VIOLATIONS_MULTI_CORNER is set to an illegal value 'value'. Legal value are true, false, 0 or 1. | 
| None | MIN_TIMING_VIOLATIONS_FAST_HV_LT is set to an illegal value 'value'. Legal value are true, false, 0 or 1. | 
Supported Families
| Supported Families | 
|---|
| PolarFire® | 
| PolarFire SoC | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
Example
The following example specifies text as the Report format and turns on report generation for Constraint_coverage report, the Max_Delay_Analysis Timing Report based on Slow process, Low Voltage, and High Temperature and the Max_Delay_Analysis Timing Violation Report based on Slow Process, Low Voltage, and High Temperature operating conditions. The script turns off Min_Delay_Analysis Timing Violation Report generation based on Slow process, Low Voltage, and High Temperature operating conditions. It also sets the maximum number of timing paths to 25 and maximum slack threshold of 0.04:
configure_tool -name {VERIFYTIMING} \
               -params {FORMAT:txt} \
               -params {CONSTRAINT_COVERAGE:1} \
               -params {MAX_TIMING_SLOW_LV_HT:1} \
               -params {MAX_TIMING_VIOLATIONS_SLOW_LV_HT:1} \
               -params {MIN_TIMING_VIOLATIONS_SLOW_LV_HT:0}
               -params {MAX_PATHS_TIMING:25} \
               -params {SLACK_THRESHOLD_VIOLATION:0.04}
		    
run_tool -name {VERIFYTIMING} -script {timing.tcl}Sample SmartTime Tcl Script <timing.tcl>
# Create user path set -from B_reg 
create_set -name from_B_reg \
    -source {B_reg*[*]:CLK} -sink {*}
# Create user set -from A, B, C
create_set -name from_in_ports \
    -source {A B C} \
    -sink {*}
# Generate Timing Reports
report \
    -type timing \
    -analysis min \
    -format text \
    -max_paths 10 \
    -print_paths yes \
    -max_expanded_paths 10 \
    -include_user_sets yes \
    min_timing.rpt
# Export SDC
write_sdc -scenario {Primary} exported.sdc
#save the changes
save