TCPIP_HTTP_FileInclude Function
C
void TCPIP_HTTP_FileInclude(
HTTP_CONN_HANDLE connHandle,
const uint8_t* cFile
);
Description
This function allows an entire file to be included as a dynamic variable, providing a basic templating system for HTML web pages. This reduces unneeded duplication of visual elements such as headers, menus, etc.
When pHttpCon->callbackPos is 0, the file is opened and as many bytes as possible are written. The current position is then saved to pHttpCon->callbackPos and the file is closed. On sobsequent calls, reading begins at the saved location and continues. Once the end of the input file is reached, pHttpCon->callbackPos is set back to 0 to indicate completion.
Preconditions
None.
Parameters
| Parameters | Description |
|---|---|
| connHandle | HTTP connection handle. |
| cFile | The name of the file to be sent. |
Returns
None.
Remarks
Users should not call this function directly,but should instead add dynamic variables in the form of inc:filename.ext in their HTML code to include the file at that specified location (for example, "filename.ext"). The mpfs2.jar utility will handle the rest.