HTTP_STATUS Enumeration
C
typedef enum {
HTTP_GET = 0u,
HTTP_POST,
HTTP_BAD_REQUEST,
HTTP_UNAUTHORIZED,
HTTP_NOT_FOUND,
HTTP_OVERFLOW,
HTTP_INTERNAL_SERVER_ERROR,
HTTP_NOT_IMPLEMENTED,
HTTP_REDIRECT,
HTTP_SSL_REQUIRED,
HTTP_MPFS_FORM,
HTTP_MPFS_UP,
HTTP_MPFS_SIGNATURE,
HTTP_MPFS_OK,
HTTP_MPFS_WAIT,
HTTP_MPFS_ERROR
} HTTP_STATUS;
Description
Supported commands and server response codes.
Members
| Members | Description |
|---|---|
| HTTP_GET = 0u | GET command is being processed. |
| HTTP_POST | POST command is being processed. |
| HTTP_BAD_REQUEST | 400 Bad Request will be returned. |
| HTTP_UNAUTHORIZED | 401 Unauthorized will be returned. |
| HTTP_NOT_FOUND | 404 Not Found will be returned. |
| HTTP_OVERFLOW | 414 Request-URI Too Long will be returned. |
| HTTP_INTERNAL_SERVER_ERROR | 500 Internal Server Error will be returned. |
| HTTP_NOT_IMPLEMENTED | 501 Not Implemented (not a GET or POST command). |
| HTTP_REDIRECT | 302 Redirect will be returned. |
| HTTP_SSL_REQUIRED | 403 Forbidden is returned, indicating SSL is required. |
| HTTP_MPFS_FORM | Show the MPFS Upload form. |
| HTTP_MPFS_UP | An MPFS Upload is being processed. |
| HTTP_MPFS_SIGNATURE | MPFS Upload looking for signature. |
| HTTP_MPFS_OK | An MPFS Upload was successful. |
| HTTP_MPFS_WAIT | An MPFS Upload waiting for the write operation to complete. |
| HTTP_MPFS_ERROR | An MPFS Upload was not a valid image. |