TCPIP_HTTP_CurrentConnectionUserDataGet Function
C
const void* TCPIP_HTTP_CurrentConnectionUserDataGet(
HTTP_CONN_HANDLE connHandle
);
Description
This function returns the user data value for the current HTTP connection. This data belongs to the user and is not used in any way by the HTTP server module. It can be set by the user with TCPIP_HTTP_Current ConnectionUserDataSet();
Preconditions
None.
Parameters
| Parameters | Description |
|---|---|
| connHandle | HTTP connection handle. |
Returns
User data that's store as part of the connection.
Remarks
None.
Example
uint32_t myConnData;
myConnData = (uint32_t)TCPIP_HTTP_CurrentConnectionUserDataGet(connHandle);