TCPIP_HTTP_CurrentConnectionHasArgsGet Function
C
uint8_t TCPIP_HTTP_CurrentConnectionHasArgsGet(
HTTP_CONN_HANDLE connHandle
);
Description
The function will get the value of the "cookies or get arguments" that are present.
Preconditions
None.
Parameters
| Parameters | Description |
|---|---|
| connHandle | HTTP connection handle. |
Returns
The current value of the connection hasArgs.
Remarks
None.
Example
uint8_t hasArgs = TCPIP_HTTP_CurrentConnectionHasArgsGet(connHandle);