TCPIP_HTTP_PostReadPair Macro
C
#define TCPIP_HTTP_PostReadPair(connHandle, cData, wLen) TCPIP_HTTP_PostValueRead(connHandle, cData, wLen)
Description
Reads a name and value pair from a URL encoded string in the TCP buffer. This function is meant to be called from a TCPIP_HTTP_PostExecute callback to facilitate easier parsing of incoming data. This function also precents buffer overflows by forcing the programmer to indicate how many bytes are expected. At least 2 extra bytes are needed in cData over the maximum length of data expected to be read.
This function will read until the next '&' character, which indicates the end of a value parameter. It assumes that the front of the buffer is the beginning of the name parameter to be read. This function properly updates the connection byteCount (see TCPIP_HTTP_CurrentConnectionByteCountGet()) by decrementing it by the number of bytes read. It also removes the delimiting '&' from the buffer. Once complete, two strings will exist in the cData buffer. The first is the parameter name that was read, while the second is the associated value.
Preconditions
The front of the TCP buffer is the beginning of a name parameter, and the rest of the TCP buffer contains a URL-encoded string with a name parameter terminated by a '=' character and a value parameter terminated by a '&'.
Parameters
| Parameters | Description |
|---|---|
| connHandle | HTTP connection handle. |
| cData | Where to store the name and value strings once they are read. |
| wLen | How many bytes can be written to cData. |
Returns
HTTP_READ_OK - Name and value were successfully read.
HTTP_READ_TRUNCTATED - Entire name and value could not fit in the buffer, so input was truncated and data has been lost.
HTTP_READ_INCOMPLETE - Entire name and value was not yet in the buffer, so call this function again later to retrieve.
Remarks
This function is aliased to TCPIP_HTTP_PostValueRead, since they effectively perform the same task. The name is provided only for completeness.