DRV_ETHPHY_VENDOR_WOL_CONFIGURE Type
C
typedef void (* DRV_ETHPHY_VENDOR_WOL_CONFIGURE)(const struct DRV_ETHPHY_OBJECT_BASE_TYPE* pBaseObj, DRV_HANDLE handle, unsigned char bAddr[]); Returns
None
Description
Pointer to Function: typedef void (* DRV_ETHPHY_VENDOR_WOL_CONFIGURE) ( const struct DRV_ETHPHY_OBJECT_BASE_TYPE* pBaseObj, DRV_HANDLE handle, unsigned char bAddr); This type describes a pointer to a function that configures the PHY WOL functionality of the Ethernet PHY. Configures the WOL of the PHY with a Source MAC address or a 6 byte magic packet mac address. This configuration function is PHY specific and every PHY driver has to provide their own implementation.
Remarks
The PHY driver consists of 2 modules:
the main/base PHY driver which uses standard IEEE PHY registers
the vendor specific functionality This function provides vendor specific functionality. Every PHY driver has to expose this vendor specific function as part of its interface. Traditionally the name used for this function is DRV_EXTPHY_WOLConfiguration but any name can be used. The PHY driver will call the vendor set up functions after the communication to the PHY has been established. The function can use all the vendor specific functions to store/retrieve specific data or start SMI transactions (see Vendor Interface Routines). The function should not block but return DRV_ETHPHY_RES_PENDING if waiting for SMI transactions. This feature is not currently supported for all PHYs.
Preconditions
Communication to the PHY should have been established.