DRV_ETHPHY_ClientOperationAbort Function
C
DRV_ETHPHY_RESULT DRV_ETHPHY_ClientOperationAbort(DRV_HANDLE handle); Returns
DRV_ETHPHY_RESULT value describing the current operation result: DRV_ETHPHY_RES_OK for success; operation has been aborted an DRV_ETHPHY_RESULT error code if the operation failed.
Description
Aborts a current client operation initiated by the Ethernet PHY driver.
Remarks
None
Preconditions
The DRV_ETHPHY_Initialize routine must have been called.
DRV_ETHPHY_Open must have been called to obtain a valid opened device handle.
A driver operation was started