DRV_ETHPHY_Close Function
C
void DRV_ETHPHY_Close(DRV_HANDLE handle); Returns
None
Description
This function closes an opened instance of the Ethernet PHY driver, invalidating the handle.
Remarks
After calling this routine, the handle passed in "handle" must not be used with any of the remaining driver routines. A new handle must be obtained by calling DRV_ETHPHY_Open before the caller may use the driver again.
Usually there is no need for the driver client to verify that the Close operation has completed.
Preconditions
The DRV_ETHPHY_Initialize routine must have been called for the specified Ethernet PHY driver instance. DRV_ETHPHY_Open must have been called to obtain a valid opened device handle.