1.2.5.2.48 TCPIP_MAC_RX_FILTER_TYPE Enumeration
C
typedef enum {
TCPIP_MAC_RX_FILTER_TYPE_BCAST_ACCEPT,
TCPIP_MAC_RX_FILTER_TYPE_MCAST_ACCEPT,
TCPIP_MAC_RX_FILTER_TYPE_UCAST_ACCEPT,
TCPIP_MAC_RX_FILTER_TYPE_UCAST_OTHER_ACCEPT,
TCPIP_MAC_RX_FILTER_TYPE_RUNT_REJECT,
TCPIP_MAC_RX_FILTER_TYPE_RUNT_ACCEPT,
TCPIP_MAC_RX_FILTER_TYPE_CRC_ERROR_REJECT,
TCPIP_MAC_RX_FILTER_TYPE_CRC_ERROR_ACCEPT,
TCPIP_MAC_RX_FILTER_TYPE_MCAST_HASH_ACCEPT,
TCPIP_MAC_RX_FILTER_TYPE_UCAST_HASH_ACCEPT,
TCPIP_MAC_RX_FILTER_TYPE_MAXFRAME_ACCEPT,
TCPIP_MAC_RX_FILTER_TYPE_ALL_ACCEPT,
TCPIP_MAC_RX_FILTER_TYPE_FRAMEERROR_ACCEPT,
TCPIP_MAC_RX_FILTER_TYPE_JUMBOFRAME_ACCEPT,
TCPIP_MAC_RX_FILTER_TYPE_DEFAULT
} TCPIP_MAC_RX_FILTER_TYPE;
Description
MAC RX Filter Types.
This enumeration defines the RX filtering capabilities for the TCP/IP MAC driver.
Members
Members | Description |
---|---|
TCPIP_MAC_RX_FILTER_TYPE_BCAST_ACCEPT | Broadcast packets are accepted. |
TCPIP_MAC_RX_FILTER_TYPE_MCAST_ACCEPT | Multicast packets are accepted. |
TCPIP_MAC_RX_FILTER_TYPE_UCAST_ACCEPT | Unicast packets to this host are accepted. |
TCPIP_MAC_RX_FILTER_TYPE_UCAST_OTHER_ACCEPT | Unicast packets to a different host are accepted |
TCPIP_MAC_RX_FILTER_TYPE_RUNT_REJECT | Runt packets (< 64 bytes) are rejected. |
TCPIP_MAC_RX_FILTER_TYPE_RUNT_ACCEPT | Runt packets (< 64 bytes) are accepted. |
TCPIP_MAC_RX_FILTER_TYPE_CRC_ERROR_REJECT | Packets with CRC errors are rejected. |
TCPIP_MAC_RX_FILTER_TYPE_CRC_ERROR_ACCEPT | Packets with CRC errors are accepted. |
TCPIP_MAC_RX_FILTER_TYPE_MCAST_HASH_ACCEPT | Multicast HASH matching packets are accepted. |
TCPIP_MAC_RX_FILTER_TYPE_UCAST_HASH_ACCEPT | Unicast HASH matching packets are accepted. |
TCPIP_MAC_RX_FILTER_TYPE_MAXFRAME_ACCEPT | Maximum frame size packets(1536 bytes) are accepted. |
TCPIP_MAC_RX_FILTER_TYPE_ALL_ACCEPT | All packets are accepted. |
TCPIP_MAC_RX_FILTER_TYPE_FRAMEERROR_ACCEPT | Packets with Frame error are accepted. |
TCPIP_MAC_RX_FILTER_TYPE_JUMBOFRAME_ACCEPT | Packets with JUMBO Frame (up to 10240 bytes) is accepted. |
TCPIP_MAC_RX_FILTER_TYPE_DEFAULT | Default RX filter: will accept most valid packets. |
Remarks
The Ethernet/Wi-Fi controllers have an RX filter module that takes part in the packet acceptance decision.
Multiple values can be OR-ed together.
There usually is a priority in the RX filter processing for a MAC module. In order for a packet to be accepted, it has to be specifically accepted by a filter. Once a filter accepts or rejects a packet, further filters are not tried. If a packet isn't rejected/accepted after all filters are tried, it will be rejected by default.
Not all MACs support all the RX filter types.
Current implementation does not suport more than 16 filters.