IPV6_EVENT_TYPE Enumeration

C

typedef enum {
IPV6_EVENT_ADDRESS_ADDED = 1,
IPV6_EVENT_ADDRESS_REMOVED,
IPV6_EVENT_ULA_ADDRESS_GENERATED,
IPV6_EVENT_ULA_ADDRESS_FAILED
} IPV6_EVENT_TYPE;

Description

Enumeration: IPV6_EVENT_TYPE.

These events are used while notifying to the registered applications.

Members

MembersDescription
IPV6_EVENT_ADDRESS_ADDED = 1Event is generated when IPv6 added to the list.
IPV6_EVENT_ADDRESS_REMOVEDEvent is generated when IPv6 address removed from the list.
IPV6_EVENT_ULA_ADDRESS_GENERATEDEvent is generated when IPv6 unique local address included to the list.
IPV6_EVENT_ULA_ADDRESS_FAILEDEvent is generated when IPv6 unique local address is failed.

Remarks

None.