IPV6_PACKET_ACK_FNC Type

C

typedef bool (* IPV6_PACKET_ACK_FNC)(void*, bool, const void*);

Description

Type: IPV6_PACKET_ACK_FNC.

Packet allocation and deallocation acknowledgment callback function.

Parameters

ParametersDescription
void *Pointer to the packet that was transmitted.
boolTrue if the packet was sent, False otherwise.
const void*0.

Returns

  • True - If the packet needs the queuing flags removed (it is not deleted and still in use).

  • False - If the packet does not need the queuing flags removed (either no longer exists or the flags updated).

Remarks

None.