TCPIP_IPV6_MulticastListenerAdd Function

C

IPV6_ADDR_STRUCT * TCPIP_IPV6_MulticastListenerAdd(
    TCPIP_NET_HANDLE hNet, 
    IPV6_ADDR * address
);

Description

This function is used to add the IPv6 multicast address to an interface.

Preconditions

TCPIP_IPV6_Initialize() should be called. TCPIP_IPV6_InterfaceIsReady should be true.

Parameters

ParametersDescription
netHThe interface to add the address.
addressThe address.

Returns

IPV6_ADDR_STRUCT *

  • On Success - Pointer to the new listener.

  • On Failure - NULL.

Remarks

None.