TCPIP_IPV6_InterfaceIsReady Function

C

bool TCPIP_IPV6_InterfaceIsReady(
    TCPIP_NET_HANDLE netH
);

Description

Returns the current state of the IPv6 interface (i.e., determines if an interface is ready for IPv6 transactions).

Preconditions

None.

Parameters

ParametersDescription
netHThe interface to check.

Returns

  • True - If the interface has IPv6 functionality available.

  • False - If the interface does not have IPv6 functionality available.

Remarks

None.