TCPIP_IPV6_DestAddressSet Function
C
void TCPIP_IPV6_DestAddressSet(
IPV6_PACKET * p,
const IPV6_ADDR * addr
);
Description
This API is used to configure the destination address for an IPv6 packet.
Preconditions
TCPIP_IPV6_Initialize() should be called. TCPIP_IPV6_InterfaceIsReady should be true.
Parameters
Parameters | Description |
---|---|
p | Pointer to IPv6 packet. |
addr | Destination address. |
Returns
None.
Remarks
None.