17.2.16 Naked Function Attribute
The
naked attribute instructs the compiler to generate no prologue
or epilogue code for the function. This attribute is intended for functions that
exclusively contain extended inline assembly code. Using C code within such an
attributed function might not work properly. Since the compiler will not generate
prologue or epilogue code for functions using this attribute, the application code
within is responsible for managing the stack and additionally handling formal
parameters, return values, and the function return. For
example:void __attribute__ ((naked)) foo(void);