17.2.28 Tcm Function Attribute
The
tcm attribute instructs the compiler to place
the function in tightly-coupled memory (TCM), if possible, providing highly
consistent access times. The actual section will be determined by the compiler,
possibly based on other attributes such as space. For
example:void __attribute__((tcm)) foo (void) {return;}In the above example, the compiler will attempt to place
foo in the itcm memory section, or the
tcm section on those processors where the code and data
memory spaces are combined. Note that the amount of TCM available in program or
data memory on the target device may vary, so the compiler cannot ensure all
functions with the tcm attribute can be placed in TCM.
Also see Tightly-Coupled Memories.