17.2.9 Format Function Attribute
format (type, format_index,
first_to_check) attribute
indicates that the function takes a printf,
scanf, strftime, or
strfmon style format string and arguments and that
the compiler should type check those arguments against the format string,
just as it does for the standard library functions, for
example:extern int __attribute__ ((format (printf, 2, 3))) my_printf (void *my_object, const char *my_format, ...);
The type parameter is one of
printf, scanf,
strftime or strfmon (optionally
with surrounding double underscores, for example,
__printf__) and determines how the format string
will be interpreted.
The format_index parameter specifies which
function parameter is the format string. Function parameters are numbered
from the left-most parameter, starting from 1.
The first_to_check parameter specifies which
parameter is the first to check against the format string. If
first_to_check is zero,
type checking is not performed and the compiler only checks the format
string for consistency (for example, vfprintf).