17.2.6 Copy Function Attribute
The
copy(func) attribute is used to apply a set
of attributes to a function. This set is derived from the attributes applied
to the argument func. This is particularly
useful in libraries that define aliases, ensuring that the aliases have the
same attributes as the original symbols. It's important to note that the
copy attribute only duplicates syntactic and
semantic attributes. It does not copy attributes that influence a symbol's
linkage or visibility, such as alias or
weak. Additionally, the deprecated
attribute is not copied. For
example:#define StrongAlias(TargetFunc, AliasDecl) \
extern __typeof__ (TargetFunc) AliasDecl \
__attribute__ ((alias (#TargetFunc), copy (TargetFunc)));
extern __attribute__ (malloc, pure)) void* allocate (size_t);
StrongAlias (allocate, alloc);