17.2.3 Alias Function Attribute
The
alias ("symbol") attribute indicates that
the function is an alias for another symbol. For
example:void foo (void) { /* stuff */ }
__attribute__ ((alias("foo"))) void bar (void);The symbol bar is considered to be an alias for the symbol
foo.