17.2.21 Optimize Function Attribute

The optimize(optimization) attribute allows a function to be built with optimizations that differ from what has been specified on the command line and which will be applied to the rest of the program. The optimization argument can either be a number or a string. String arguments represent the command-line option used to control an optimization, for example, to enable peephole optimizations (-fpeephole), use optimize("peephole"). The -f option prefix does not need to be specified with the argument. If you want to specify more than one optimization, separate the arguments with commas but with no space characters. Arguments that begin with O are assumed to be an optimization level option, for example optimize("O1,unroll-loops") turns on level 1 optimizations and the unroll-loops optimizations (controlled by the -funroll-loops command-line option). A numerical argument is also assumed to be an optimization level, for example optimize(3) turns on level 3 optimizations and is equivalent to the full usage of the attribute in the following example.
int __attribute__((optimize("O3"))) pandora (void) {
  if (maya > axton)
    return 1;
  return 0;
}
This feature can be used, for instance, to have frequently executed functions compiled with more aggressive optimization options that produce faster and larger code, while other functions can be called with less aggressive options. Typically, however, it is not used for production builds.