17.2.32 Unused Function Attribute
The
unused attribute indicate to the compiler that the function
may not be used. The compiler will not issue a warning for this function if
it is not used, for
example:void __attribute__ ((unused)) opt_setting(void);