4.10.1.7.1 Switch RMON Statistics Configuration
Configure RMON Statistics table on the RMON Statistics Configuration page. The entry index key is ID.
The RMON Statistics Configuration page has the following parameters:
- Delete: Check to delete the entry. It is deleted during the next save.
- ID: Indicates the index of the entry. The range is from 1–65535.
- Data Source: Indicates the port ID which wants to be monitored. If in stacking switch, the value must add 1000000*(switch ID-1). For example, if the port is switch 3 port 5, then the value is 2000005.