4.10.1.7.3 Switch RMON Alarm Configuration
Configure the RMON Alarm table on the RMON Alarm Configuration page, as shown in the following figure. The entry index key is ID.
The RMON Alarm Configuration page has the following parameters:
- Delete: Check to delete the entry. It is deleted during the next save.
- ID: Indicates the index of the entry. The range is from 1–65535.
- Interval: Indicates the interval in seconds for sampling and comparing the rising and falling threshold. The range is from 1 to 2^31-1.
- Variable: Indicates the variable to be sampled. The following is the list of possible variables.
- InOctets: The total number of octets received on the interface, including framing characters
- InUcastPkts: The number of uni-cast packets delivered to a higher-layer protocol
- InNUcastPkts: The number of broad-cast and multi-cast packets delivered to a higher-layer protocol
- InDiscards: The number of inbound packets that are discarded even if the packets are normal
- InErrors: The number of inbound packets that contained errors preventing them from being deliverable to a higher-layer protocol
- InUnknownProtos: The number of the inbound packets that were discarded because of the unknown or un-support protocol
- OutOctets: The number of octets transmitted out of the interface, including framing characters
- OutUcastPkts: The number of uni-cast packets that request to transmit
- OutNUcastPkts: The number of broadcast and multicast packets that request to transmit
- OutDiscards: The number of outbound packets that are discarded even if the packets are normal
- OutErrors: The number of outbound packets that could not be transmitted because of errors
- OutQLen: The length of the output packet queue (in packets)
- Sample Type: The method of sampling the selected variable and calculating the value to be compared against the thresholds. The following is the list of sample types.
- Absolute: Get the sample directly
- Delta: Calculate the difference between samples (default)
- Value: The value of the statistics during the last sampling period
- Startup Alarm: The method of sampling the selected variable and calculating the value to be compared against the thresholds. The following is the list of sample types.
- Rising: Trigger alarm when the first value is larger than the rising threshold
- Falling: Trigger alarm when the first value is less than the falling threshold
- RisingOrFalling: Trigger alarm when the first value is larger than the rising threshold or less than the falling threshold (default).
- Rising Threshold: Rising threshold value (−2147483648 to 2147483647)
- Rising Index: Rising event index (0–65535). If this value is zero, then no associated event is generated, as zero is not a valid event index.
- Falling Threshold: Falling threshold value (−2147483648 to 2147483647)
- Falling Index: Falling event index (0–65535). If this value is zero, no associated event is generated, as zero is not a valid event index.