4.10.2.3.1 Network ACL Ports Configuration
Configure the ACL parameters (ACE) of each switch port, as shown in the following figure. These parameters affect frames received on a port unless the frame matches a specific ACE.
The ACL Ports Configuration page has the following parameters:
- Port: The logical port for the settings contained in the same row
- Policy ID: Select the policy to apply to this port. The allowed values are 0–63. The default value is 0.
- Action: Select if forwarding is permitted (Permit) or denied (Deny). The default value is Permit.
- Rate Limiter ID: Select which rate limiter to apply on this port. The allowed values are Disabled or the values 1–16. The default value is Disabled.
- Port Redirect: Select which port frames are redirected. The allowed values are Disabled, or a specific port number and it cannot be set when action is permitted. The default value is Disabled.
- Mirror: Specify the mirror
operation of this port. The allowed values are:
-
Enabled: Frames received on the port are mirrored
-
Disabled: Frames received on the port are not mirrored
The default value is Disabled.
-
- Logging: Specify the logging
operation of this port. Notice that the logging message does not include the 4 bytes
CRC. The allowed values are:
-
Enabled: Frames received on the port are stored in the System Log
-
Disabled: Frames received on the port are not logged
The default value is Disabled.
Note: The logging feature only works when the packet length is less than 1518 (without VLAN tags) and the System Log memory size and logging rate is limited.
-
- Shutdown: Specify the port
shut down operation of this port. The allowed values are:
-
Enabled: If a frame is received on the port, the port is disabled
-
Disabled: Port shut down is disabled
The default value is Disabled.
Note: The shutdown feature only works when the packet length is less than 1518 (without VLAN tags).
-
- State: Specify the port state
of this port. The allowed values are:
- Enabled: To reopen ports by changing the volatile port configuration of the ACL user module
- Disabled: To close ports by changing the
volatile port configuration of the ACL user module
The default value is Enabled.
- Counter: Counts the number of frames that match this ACE.