8.9 Understanding Bottleneck Reports -
SmartFusion2, IGLOO2, RTG4, and PolarFire
A bottleneck is a point in the design that contributes to multiple timing violations. The
Bottleneck Report lists the bottlenecks in the design. You can generate this report
from SmartTime Analyzer.
Note: The bottleneck can be computed only when a cost type is
defined. There are two cost type options available:
Path count: associates
the severity of the bottleneck to the count of violating/critical paths that
traverse the instance.
Path cost: associates
the severity of the bottleneck to the sum of the timing violations for the
violating/critical paths that traverse the instance.
Figure 8-4. Sample Bottleneck Report
The Bottleneck Report contains the following parts:
Table 8-5. Bottleneck Report
Sections
Part
Description
Device Description
Contains general information about the design, including:
Design
name
Family
Die
Package
Software
version
Bottleneck Analysis
Lists the core of the bottleneck information. It is organized
into two columns:
Instance
Name: refers to the output pin name of the instance.
Path Count: shows the number of violating paths that include
the instance pin.