8.3 Understanding Timing Reports
| Section | Description |
|---|---|
| Header | Lists the:
|
| Summary | Reports the timing information for each clock domain. By default, the clock domains reported are the explicit clock domains that are shown in SmartTime. To filter the domains and show only specific sections in the report, use the Timing Report Options dialog box. |
| Path | Lists the timing information for different types of paths in the
design. This section is reported by default. You can deselect this
option in the Timing Report Options dialog box. By default, the number of paths displayed per set is 5. You can filter the domains using the Timing Report Options dialog box. You can also view the stored filter sets in the generated report using the Timing Report options. The filter sets are listed by name in their appropriate section. The number of paths reported for the filter set is the same as for the main sets. By default, the filter sets are not reported. |