FPU Pipeline Full or Busy
When the CPU attempts to issue an instruction to the coprocessor, and it is unable to accept it because the pipeline is full or busy, an external structural hazard will result, and the coprocessor will stall the CPU until such time that the instruction can be accepted.
When an issued instruction is stalled in the FPU RD-stage due to a RAW hazard with a prior currently executing instruction, the FPU pipeline is considered busy such that further FPU instructions cannot be accepted. Consequently, should the CPU attempt to issue any additional FPU instructions while the RD-stage is stalled, the FPU will stall the CPU until such time that the hazard resolves, resulting in an external structural hazard as shown in Figure 3-34.
The pipeline is considered full when the Instruction/Hazard Tracker FIFO is full, which occurs when the number of instructions (default value is four) are active within it, including the one waiting in the RD-stage for dispatch into X[0]. The pipeline will remain full until the oldest instruction enters the WB-stage. Should the CPU attempt to issue another FPU instruction, the FPU will stall the CPU until such time that the Instruction/Hazard Tracker FIFO is no longer full.