15.8.2 Three-Phase Sinusoidal Control of PMSM/ACIM Motors

Three-phase sinusoidal control applies voltages to the three-phase motor windings, which are pulse-width modulated to produce sinusoidal currents as the motor spins. This eliminates the torque ripple and commutation spikes associated with trapezoidal commutation. Typically, Center-Aligned Complementary PWMs are used for sinusoidal control of a Permanent Magnet Synchronous Motor (PMSM) or a three-phase AC Induction Motor (ACIM). Center-aligned PWM signals reduce the level of harmonics in output voltages and currents as compared to edge-aligned PWMs. Three PWM Generators are connected to the three-phase power bridge driving the motor, as shown in Figure 15-40.

PWM Generator 1 is configured as a host, and PWM Generator 2 and PWM Generator 3 are configured as client PWMs. PWM configuration used in three-phase sinusoidal control is summarized below:

  • PG1-PG3: Uses master period and independent duty cycles.
  • PG1-PG3: PWM Operating mode is selected as Center-Aligned mode.
  • PG1-PG3: Configured to operate in Single Trigger mode.
  • PG1-PG3: PWM Output mode is configured as Complementary Output mode.
  • PG2-PG3: Uses PG1 trigger output as Start-of-Cycle, whereas PG1 is self-triggered.
  • PG2-PG3: Enabled during initialization.
  • PG1 is enabled only after configuring all the control registers; whenever PG1 is enabled, all the generators will start in unison.

Figure 15-44 shows the PWM waveforms for a given point in time. Center-Aligned mode uses two timer cycles to produce a PWM cycle and maintains symmetry at the center of each PWM cycle. Each timer cycle can be tracked using the status bit, CAHALF (PGxSTAT[1]), of the respective PWM Generator. The leading edge is produced when CAHALF = 0, and the falling edge is produced when CAHALF = 1. Note that with Center-Aligned mode, as long as the duty cycles are different for each phase, the switching instants occur at different times. (In Edge-Aligned mode, the turn-on times are coincident.) This generally reduces electromagnetic interference.

Figure 15-44. Three-Phase Center-Aligned Waveforms

Three-Phase Sinusoidal PMSM/ACIM Motor Control Code

void PWMInitialization(void);

#include <xc.h>
#include <stdint.h>

int main(void) 
{

	PWMInitialization();  
    
    while (1)
    {
        
    }
}

void PWMInitialization(void)
{
    PCLKCON      = 0x0000;    
    
    //Set PWM master clock to 400MHz from PLL2 through CLKGEN5
    configure_PLL2_Fout_400MHz();
    clock_PWM_from_PLL2_Fout();
    
    /* PWM Clock Divider Selection bits
       0b11 = 1:16 ; 0b10 = 1:8 ;0b01 = 1:4 ; 0b00 = 1:2 */
    PCLKCONbits.DIVSEL = 0;
    /* PWM Master Clock Selection bits
       0b01 = CLKGEN5 ; 0b00 = UPB clock */
    PCLKCONbits.MCLKSEL = 1;
    /* Lock bit: 0 = Write-protected registers and bits are unlocked */
    PCLKCONbits.LOCK = 0;

    /* Initialize Master Period Register */
    MPER         = 40000;
    /* Set PWM Phase Register - No phase shift */
    MPHASE = 0;
    /* Set PWM Duty Cycles */
    PG1DC = 10000;
    PG2DC = 20000;
    PG3DC = 30000;
    /* Set Dead Time Registers */
    PG1DT = 0x06400640;
    PG2DT = 0x06400640;
    PG3DT = 0x06400640;
	
    PG1CON = 0x00000000;
    /* Select PWM Generator Duty Cycle Register as PG1DC */
    PG1CONbits.MDCSEL = 0;
    /* Select PWM Generator Period Register as MPER */
    PG1CONbits.MPERSEL = 1;
    /* Select PWM Generator Phase Register as MPHASE */
    PG1CONbits.MPHSEL = 1;
    /* PWM Generator broadcasts software set of UPDREQ *
    * control bit and EOC signal to other PWM generators. */
    PG1CONbits.MSTEN = 1;
    /* Start of Cycle is Local EOC */
    PG1CONbits.SOCS = 0;
    /* PWM Generator uses Master Clock selected by
    the PCLKCONbits.MCLKSEL bits */
    PG1CONbits.CLKSEL = 1;
    /* PWM Generator operates in Center-Aligned mode*/
    PG1CONbits.MODSEL = 4;
	
    PG1IOCON1 = 0x00000000;
    /* PWM Generator Output operates in Complementary Mode */
    PG1IOCON1bits.PMOD = 0;
    /* PWM Generator controls the PWMxH output pin */
    PG1IOCON1bits.PENH = 1;
    /* PWM Generator controls the PWMxL output pin */
    PG1IOCON1bits.PENL = 1;
    
    PG1EVT1 = 0x00000000;
    /* Time base interrupts are disabled */
    PG1EVT1bits.IEVTSEL = 3;
    /* A write of the PGxDC register automatically sets the UPDREQ bit */
    PG1EVT1bits.UPDTRG = 0;
    /* PWM generator trigger output is EOC*/
    PG1EVT1bits.PGTRGSEL = 0;
	
    PG2CON = 0x00000000;
    /* Select PWM Generator Duty Cycle Register as PG2DC */
    PG2CONbits.MDCSEL = 0;
    /* Select PWM Generator Period Register as MPER */
    PG2CONbits.MPERSEL = 1;
    /* Select PWM Generator Phase Register as MPHASE */
    PG2CONbits.MPHSEL = 1;
    /* Start of Cycle is PG1 trigger output selected by
    PG1EVTbits.PGTRGSEL<2:0> bits */
    PG2CONbits.SOCS = 1;
    /* PWM Generator uses Master Clock selected by
    the PCLKCONbits.MCLKSEL bits */
    PG2CONbits.CLKSEL = 1;
    /* PWM Generator operates in Center-Aligned mode */
    PG2CONbits.MODSEL = 4;
    
    PG2IOCON1 = 0x00000000;
    /* PWM Generator output operates in Complementary Mode */
    PG2IOCON1bits.PMOD = 0;
    /* PWM Generator controls the PWMxH output pin */
    PG2IOCON1bits.PENH = 1;
    /* PWM Generator controls the PWMxL output pin */
    PG2IOCON1bits.PENL = 1;
	
    PG3CON = 0x00000000;
    /* Select PWM Generator Duty Cycle Register as PG2DC */
    PG3CONbits.MDCSEL = 0;
    /* Select PWM Generator Period Register as MPER */
    PG3CONbits.MPERSEL = 1;
    /* Select PWM Generator Phase Register as MPHASE */
    PG3CONbits.MPHSEL = 1;
    /* Start of Cycle is PG1 trigger output selected by
    PG1EVTbits.PGTRGSEL<2:0> bits */
    PG3CONbits.SOCS = 1;
    /* PWM Generator uses Master Clock selected by
    the PCLKCONbits.MCLKSEL bits */
    PG3CONbits.CLKSEL = 1;
    /* PWM Generator operates in Center-Aligned mode */
    PG3CONbits.MODSEL = 4;
    
    

    PG3IOCON1 = 0x00000000;
    /* PWM Generator output operates in Complementary Mode */
    PG3IOCON1bits.PMOD = 0;
    /* PWM Generator controls the PWMxH output pin */
    PG3IOCON1bits.PENH = 1;
    /* PWM Generator controls the PWMxL output pin */
    PG3IOCON1bits.PENL = 1;

    /* Turning ON the PWM Generator 3 */
    PG3CONbits.ON = 1;
    /* Turning ON the PWM Generator 2 */
    PG2CONbits.ON = 1;
    /* Turning ON the PWM Generator 1;
    Thus starting all the PWM modules in unison */
    PG1CONbits.ON = 1;  
}