22.4.2.6.2 Host Mode Clocking and MCLK
The SPI module as a host has the ability to generate BCLK and LRCK by internally
generating using SPICLK (MCLKEN = 0). In addition, the 33A device can
generate the clock for external codec devices using the reference output, REFCLKO
function (see Figure 22-30), although some codecs may
have the ability to generate their own MCLK from a crystal to provide accurate audio
sample rates.
Figure 22-30 shows that the REFCLKO clock can be used as MCLKIN by the codec.
Figure 22-30 shows the interface between an SPI client and a codec host, deriving the clock from the MCLK input interface.