Connected
boolean Connected()
Returns True if Connect was successful. The IDE calls
internally Connect when, for example, you press the refresh button in
the Dashboard window.
After connection, depending on the device, the rest of the debug functions will be available.
For some devices the ready state needs to be arrived at by starting a debug session.