5.7.2 Remove a Toolchain
To remove an existing toolchain:
- Click to select the toolchain from the list.
- Click the Remove button.
This will NOT uninstall the compiler from your computer; it will only remove MPLAB X IDE awareness of this compiler. To add the toolchain back, see .
If you want to uninstall a compiler from your computer, remove the reference to the compiler in MPLAB X IDE first, as specified above. Then uninstall the compiler. If you uninstall the compiler first and then start MPLAB X IDE, the toolchain paths will appear in red. To remove the reference to this uninstalled compiler, follow the steps above.