38.3.2.2 Configuration of Scan Region
Determine the section sizes in blocks corresponding to the Flash memory page size. The sizes of these sections are set by the Boot Size (FUSE.BOOTSIZE) and Code Size (FUSE.CODESIZE) fuses. Refer to the Fuse section for more information. The Boot Loader Code (BOOT) section stretches from FLASHSTART to BOOTEND, the Application Code (APPCODE) section stretches from BOOTEND to APPEND, and the remaining is the Application Data (APPDATA) section.
If FUSE.BOOTSIZE is written to ‘0’, the entire Flash is considered the
BOOT section. If FUSE.CODESIZE is written to ‘0’ and FUSE.BOOTSIZE >
0, the APPCODE section runs from BOOTEND to the end of the Flash, meaning no APPDATA
section.
Which region to scan is configured in the CRC Source (SRC) bit field in the CRCSCAN.CTRLA register.
Starting a scan of an unconfigured Flash region will set the ERROR bit in the
CRCSCAN.STATUSA register. For starting a scan with SRC set to CODE or DATA when
BOOTSIZE=’0’ (the whole Flash is BOOT) or SRC set to DATA when
CODESIZE=’0’ (no DATA section) will both result in CRC failure.
| CRC Source | Scan Region | BOOTSIZE | CODESIZE |
|---|---|---|---|
| BOOT | BOOT | > 0 | - |
| The entire Flash | 0 | - | |
| CODE | APPCODE | > 0 | - |
| DATA | APPDATA | > 0 | BOOTEND + APPEND < FLASHEND |