15.8.1 Reading a TEF Object
Before reading a TEF object, the application must check that the TEF is not empty by reading the CxTEFSTA register. The TEF is not empty if TEFNEIF is set.
The TEF user address points to the address in RAM of the next TEF object to read. The actual address in RAM is calculated using Equation 15-25. TE0 of the TEF object is read first, followed by TE1 and TE2.
A = BaseAddress =
CxFIFOBA
After the TEF object is read from RAM, the TEF needs to be incremented by setting UINC (CxTEFCON[8]). This will cause the CAN FD Protocol module to increment the tail pointer and update CxTEFUA.
Now, the next message can be read from the TEF.