19.3.17 Math Sequencer Commands
The math post-processing sequence is called by an acquisition sequence. The internal structure of the math hardware is shown in Figure 19-9.
The sequence is finished when the END bit is set.
The arithmetic module has two inputs: AIN and BIN. For input A (AIN), the following sources can be selected:
0= Zero1= Accumulator A2= Reserved3= ADC5 Conversion Result
For input B (BIN), the following sources can be selected:
0= ITCRESx register1= Accumulator B2= Reserved3= ADC5 Conversion Result
The math sequence command executes a math operation as specified by F[1:0] bits. The following options are available:
0= data from A input is copied to the math result.1= data from B input is copied to the math result .2= the math result is a sum of B and A inputs.3= the math result is a difference between of B and A inputs.
The output of the math operation is stored in the ITCRESx register if it is defined by WM[1:0] bits of the ITCLSxCON register or by WM[1:0] bits in the SMATHCMDx command when the WMOV bit is set. Also, the math result can be latched into two accumulators when ACCA and/or ACCB bits are set.
Both accumulators A and B are reset to zero by hardware before the record’s processing is started.