4.6.3.1 Not a Number (NaN)
The Signaling NaN (sNaN) and Quiet NaN (qNaN) are specific data codes that indicate certain situations. In all cases, an exponent value of all 1’s with a non-zero mantissa signifies a NaN (an exponent value of all 1’s with an all 0’s mantissa is used to convey Infinity).
qNaNs may be generated as the result of an invalid operation, such as taking the square root of a negative floating-point number. A qNaN will propagate through subsequent floating-point operations. Operations that will generate an Invalid exception for each instruction are documented in Table 4-18.
sNaNs are reserved input operands which, under default exception handling, will signal an Invalid exception when encountered. This may be used to indicate uninitialized variables or as debug aids, but they are never generated by arithmetic computations or comparisons. Whenever the source operand of operation is an sNaN, the result will be a qNaN.
Both sNaNs and qNaNs can store “payloads” in the mantissa bit field. The payload must not affect the MSB of the mantissa. The payload can be used as a debugging aid in tracing through complex arithmetic calculations.